FTASecurity and FTA Activation Service Installed on Same Machine

Perform the following steps to create certificates:
IMPORTANT:
Create the signed certificates using the same CA used in FTASecurity.
IMPORTANT:
Ensure that proper permissions are provided to access certificates folder.
  1. Follow the “Scripts for Generating CA Signed Certificates” section in Analytics Security Provider Advanced Installation Guide (Windows) to generate certificates.
  2. Use the <FQDN-hostname>.p12 certificate generated in the FTA Security Installation process to configure the FTA Activation Service.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.