Install FT Activation Websocket Service

Install FT Activation Websocket Service

  1. Go to
    <Install_Directory>\FTAActivationService
    folder.
  2. Double-click on the
    FTActivationWebsocketServiceInstaller.msi
    file to install the FT Activation Websocket Service.
  3. Wait until the installation completes. The window will close automatically.
    Install FT Activation Websocket Service
  4. Open the Windows Services console. Ensure the FactoryTalk Activation Websocket Service is installed and running.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal