Install FTA Activation Service
NOTE:
If the FTServicePlatform is already installed, user must apply the FTSP patch. Refer to KB RAID 1092336:
https://rockwellautomation.custhelp.com/app/answers/detail/a_id/1092336
Perform the following steps to install FTA Activation Service.
- Run the DataView Advanced Installer build and go to the installation directory:<DataView_Install_Directory><FactoryTalkAnalyticsDataViewAdvanced>
- Copy the following folders to the windows system.
- FTAActivationService
- FTActivation
- To install the FTA Activation Service, install the following:
- FT Activation Manager
- FT Activation Websocket Service
Provide Feedback