Back up
- Take the backup of the websocketService.dll.config file to use the same certificate path with password, which is available in the C:\Program Files (x86)\Rockwell Automation\FactoryTalk Activation Websocket ServiceNOTE:Ensure to take backup of the<FQDN-hostname>.p12file if it is available in the above folder, the file will be deleted when the Websocket Service is uninstalled.Websocket File
- Execute the following command to delete the Activation Websocket Service:sc delete ActivationWebsocketServiceDelete Activation Websocket Service
- Execute the following command to delete the Activation Manager Service:sc delete "FactoryTalk Activation Service"Delete Activation Manager Service
Provide Feedback