Pre-Upgrade Preparation
The following steps must be performed, if the user upgrades from a previous version of FT Activation Websocket service.
To Rehost and use the existing Activation Licenses, follow the steps in the Rehost Activation section.
NOTE:
If the User does not rehost the Activation Licenses, the existing licenses still are valid and usable.
Provide Feedback