Install Third Party Software

This chapter details the installation steps for third-party components required for installing the DataView application.
Review the application components and required dependencies on each node of the preferred deployment stack (refer to “Key Components and Dependencies”). Follow the instructions in this chapter to install the required third-party components on each node. This will be the prerequisite for deployment and configuration in subsequent chapters.
NOTE:
Ensure that the ports used (if any) for third-party applications are open in the firewall.
Example:
The 5432 port is required for PostgreSQL. Therefore, this port should be enabled in the firewall.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.