CA Public Key

The certificates created using the CA are not trusted by web browsers (see below).
In order to establish trust, the root public key for the CA can be imported into the system’s trusted certificate store. This can be configured for most browsers in the advanced settings.
NOTE:
For self-signed certificates, ensure to get the root public certificate (ca.crt) from the certificate authority (CA) and import the certificate into the browser. The root public certificate (ca.crt) is available in the
C:\Users\Administrator\.fta-ca\CA directory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.