Create Storyboard

Create Storyboard

User can create a Content with different templates.
  • Basic Templates
    The following are the templates where User can create desired dataset:
    • Basic Template
    • Blank Template
  • Pre-configured Templates
    • Plant Manager Template
    • Alarms & Events Template
    • Maintenance Template
    • Supervisor Template
    • Operator Template
    NOTE:
    Refer to the
    4.01.00 FactoryTalk Analytics DataView Connectors Configuration Guide
    for steps to create Storyboard with different templates.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal