Download

Download

Allows the User to download the Storyboard in JPG format. Downloads the current state of the Storyboard even if the Storyboard is not saved, for example, the User can apply filters and download the updated Storyboard without saving the Storyboard.
  1. On the Storyboard, click the [] icon to download the Storyboard.
    Download Storyboard
    The Storyboard with all tiles is downloaded as JPG file. The downloaded file name will be the title of the Storyboard.
    Storyboard Downloaded
  2. Open the downloaded .jpg file to view the Storyboard.
    Storyboard Downloaded .jpg File
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal