Storyboard Features
This chapter describes the features available on the Storyboard. The Maximum of 15 tiles can be displayed on a Storyboard.
The menu at the top right corner on the Storyboard page provides the following options to manage the Storyboard:
- Refresh
- Sharing Options
- Quick Info
- Live Storyboard
- Filters
- Query Parameter
- Download
- Storyboard Preferences
- Save ChangesStoryboard
Provide Feedback