Refresh
Allows User to view the updated data from the source. When the dataset is large, then the Power User can click the [
] icon to sync the data into the in-memory layer for the first time after saving the Content.

The Refresh option is available for both Storyboard and the Chart.
Provide Feedback