Live Storyboard

Live Storyboard

Allows the User to view the last updated time on the Storyboard.
  1. On the Storyboard menu, click the [] icon, the Live Data panel displays. By default, [None] option is selected.
    Live Storyboard
  2. Select the [Chart Refresh Frequency] radio button and add the required frequency to update the Storyboard.
    Live Storyboard - Settings
    The update frequency duration are as follows:
    Update Frequency duration in:
    Minimum
    Maximum
    Seconds
    5 sec
    59 sec
    Minutes
    1 min
    59 min
    Hours
    1 hr
    No max validation
  3. Click [Apply] the ‘Live settings applied successfully’ message displays.
  4. Storyboard with last updated time displays and refreshes as per the chart refresh frequency settings.
    NOTE:
    The Live icon [] displays on the chart tiles that are created with the same dataset.
    Live Storyboard
    NOTE:
    Ensure to sets the Chart Refresh Frequency interval more than session time-out.
  5. Click [Save Changes] to save the Storyboard with the applied refresh frequency settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal