Configuring
Data Providers
FactoryTalk InfoPlatform
can connect to data sources via components called Data Providers.
The product is installed with default data providers that connect
to FTHistorians and OpcDa data sources as well as a built-in data
simulator. Connectivity can be easily extended by installing custom
data providers into the installation folder and editing the configuration
file as described below.
Provide Feedback