Configure
FactoryTalk InfoPlatform Service
The installation places
files by default to the following folder:
C:\Program Files
(x86)\Rockwell Software\FactoryTalk Analytics InfoPlatform Service
Features of the service can be modified by
editing the configuration file located in this folder:
RA.InfoPlatform.WindowsService.exe.config
Example configurations are provided in the
appendices.
Provide Feedback