Simulator
In addition to Historians, the InfoPlatform service includes a
Simulator
data provider that can be useful for development or debugging purposes.The following entry in the config file must be included for the simulator data provider to be enabled:
|
The diagram below shows a sample representation of the name space including the Simulator.
Tags
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/infoplatform-guide-01/configure-infoplatform-service/30simulator.png/_jcr_content/renditions/original)
Provide Feedback