Configure FTEGInfluxDB in FTA InfoPlatform Service
To enable the connector user has to add the following xml structure to the "FactoryTalk Analytics InfoPlatform Service" configuration file ("RA.InfoPlatform.WindowsService.exe.config").
<PlugIns> <add assembly="RA.InfoPlatform.InfluxDB2Provider" type="RA.InfoPlatform.InfluxDB2Provider.PlugIn"> <Parameters> <add name="ConfigFile" value="InfluxDB2-Plugin.config" /> </Parameters> </add> </PlugIns>
With three parameters user can specify the behavior of the connector:
Property Name | Description |
---|---|
ConfigFile | Defines the file that should be used to configure the InfluxDB server connections. |
- Define a Connection to FTEGInfluxDB ServerAll FTEGInfluxDB connections are defined in the InfluxDB2-Plugin.config configuration file (JSON format). For connect to FTEGInfluxDB datasource user should provide connection string into InfluxDB2-plugin.config. For Example:[ { "InstanceName": "InfluxDB2-Server-1", "ServerUrl": "http://<hostname>:8086", "Authorization": "7GIJDEWHZoLwfGpXEqYxxrg3O2TmxoXFVDsjfh_QA4OBpQgwiK6ZPM1vDPv2e-2E7cgkOEBdkERBOW bhLhMwVw==", "BucketName": “Demobucket”, "PasswordEncrypted": false } ]
Property Name | Description |
---|---|
InstanceName | This will be unique instance name of Connection |
ServerUrl | Provide InfluxDB2 server URL with port based on the configuration. http://<hostname>:<port> |
Authorization | It will hold Token code with all privilleges (must) to access Bucket. |
BucketName | This will hold specific bucket name to map into database and display in navigation. Mapped database name will be same as bucket name. |
PasswordEncrypt ed | Default value will be false. Token code will be encrypt after service restart |
Provide Feedback