Verify FTEGInfluxDB Tags
Perform the following steps to verify the Tags:
- Log in to DataView application, click [Add Connections] the Connect dialog displays.
- Select FactoryTalk Service under the 'To Service' section.
- Enter the parameters and click [Test Connection]. If all the details are valid, the “Connection Success” message displays.Test Connection
- Verify the list of FTEGInfluxDB tags available under FactoryTalk Edge Gateway Model.FTEGInfluxDB Tags
Provide Feedback