Configure
InfluxDB in FTA InfoPlatform Service
To enable the connector
user has to add the following xml structure to the “FactoryTalk
Analytics InfoPlatform Service” configuration file (“RA.InfoPlatform.WindowsService.exe.config”).
<PlugIns> <add assembly="RA.InfoPlatform.InfluxDbProvider" type="RA.InfoPlatform.InfluxDbProvider.PlugIn"> <Parameters> <add name="ConfigFile" value="InfluxDB-Plugin.config"
/> <add name="FolderName"
value="InfluxDB" /> </Parameters> </add> </PlugIns> |
With three parameters user can specify the
behavior of the connector:
Property Name | Description |
---|---|
ConfigFile | Defines the file that
should be used to configure the InfluxDB server connections. |
FolderName | The name of the root
folder that contains all InfluxDB connector instances. |
Provide Feedback