Define a Connection to InfluxDB Server

Define a Connection to InfluxDB Server

All InfluxDB connections are defined in the
InfluxDB-Plugin.config
configuration file (JSON format). In the following example are two InfluxDB connections defined:
[
{
"InstanceName": "InfluxDB-Server-1",
"ServerUrl": "http://192.168.1.162:8086",
"SubscriptionIpAddress": "",
"SubscriptionPort": 9098,
"User": "InfoPlatform",
"Password": "InfluxDBPW",
"PasswordEncrypted": false
},
{
"InstanceName": "InfluxDB-Server-2",
"ServerUrl": "http://192.168.1.221:8086",
"SubscriptionIpAddress": "192.168.1.200",
"SubscriptionPort": 9099,
"User": "tk",
"Password": "secret",
"PasswordEncrypted": false
}
]
Property Name
Description
InstanceName
Name of the InfluxDB connector in the model.
ServerUrl
Server URL in the following form:
http://<hostname>:<port>
SubscriptionIpAddress
The InfluxDB connector provides a web server to get informed by InfluxDB of a field or a tag values change. This property defines the ip address. If this property will be blank, the connector tries to detect the IP address automatically.
SubscriptionPort
The InfluxDB connector provides a web server to get informed by InfluxDB of a field or a tag values change. This property defines the used port.
User
User
Password
Password
PasswordEncrypted
If the password is added in the configuration file, user can do this in plain text. Set the parameter to false and the password will be encrypted automatically at the first start.
  1. Restart InfoPlatform service.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal