Enable OPC UA Connector

Perform the following steps to enable the OPC UA connector in the FTA InfoPlatform Service.
Add the following xml structure to the "FactoryTalk Analytics InfoPlatform Service" configuration file ("RA.InfoPlatform.WindowsService.exe.config").
<PlugIns>
<add assembly="RA.InfoPlatform.OpcUaProvider"
type="RA.InfoPlatform.OpcUaProvider.PlugIn">
<Parameters>
<add name="ConfigFile" value="OPCUA-Plugin.config" />
<add name="FolderName" value="OPCUA" />
<add name="CertificateValidationOption" value="AcceptOnce" />
</Parameters>
</add>
</PlugIns>
With three parameters user can specify the behavior of the connector:
Property Name
Description
ConfigFile
Defines the file that should be used to configure the OPC UA server connections. Refer “Define Connection to OPC UA Server” section.
FolderName
The name of the root folder that contains all OPC UA connector instances.
CertificationValidationOption
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.