Connect
OSI PI Server
Perform the following
steps to connect OSI PI Server (Version 2017 R2):
- If the PI AF SDK is used to connect from InfoPlatform. Then the InfoPlatform can connect to both Historian SE and OSI PI servers.
- OSI PI Servers will show up under the folder called "Historians" when browsing rather than under the folder called "FTdirectory" (This is indicated in the InfoPlatform configuration manual).
- OSI PI customers may have to pay OSI for third party access if they don't have an enterprise agreement with OSI.
- FactoryTalk Historian ME connectivity is not supported through the InfoPlatform connector. FactoryTalk Historian ME data can be rolled up to a FactoryTalk Historian SE server and then accessed by InfoPlatform.
Provide Feedback