Verify PI Asset Framework
- Log in to DataView application, click [Add Connections] the Connect dialog displays. Select FactoryTalk Service under the ‘To Service’ section.
- Enter the parameters and Click [Test Connection]. If all the details are valid, the “Connection Success” message displays.Test Connection
- Verify the list of databases, elements available under Factory Talk Service model. DataView enables User to import and analyse EventFrames information from PIAF tags and create Storyboard.NOTE:The element tags without child items are hidden under PIAF tag hierarchy, but there is no change in the Database.PIAF Tags
Provide Feedback