Install OSIsoft PI SDK
To connect InfoPlatform with Historian install the following:
To install the OSIsoft’s PI SDK, run the setup from the media as specified in the section: “InfoPlatform Service Installation Package”
Refer to OSIsoft documentation for additional information.
Provide Feedback