Import User
Perform the following steps to import a User:
- Click [Manage Users] on the left panel.
- Click the IMPORT USERS tab.
- On the Import Users page, search for the list of Users that are not imported into DataView. This list should include the User (for example: user2) created earlier.
- Select the User to import (for example: user2).
- Select [Design User] from the Select Role Name drop-down list.
- Click [Add].
The “User imported successfully” message displays.
After the successful update, the imported user (for example: user2) can use the DataView application.
Provide Feedback