Create
DataFlowML User
To add other Users,
follow the same steps used to create Superuser, but use different
User names and add the new Users to the DataFlowML Users Group.
NOTE:
When a User is created ensure
to configure email.
Create a new Workspace in DataFlowML with the
User that was created in the Analytics Security Provider.
NOTE:
Refer the FactoryTalk Analytics
DataFlowML Administration Guide to create a new Workspace and assign
each User to the Workspace.
Provide Feedback