Private
Network without a domain or Domain Name Server (DNS)
CA signed certificates
require the use of fully qualified domain names. In cases where
there is no domain or there is no domain name server there are two
options. The first and best option is to use hosts files instead
to map the IP addresses to qualified host names. The second is to
use self-signed certificates instead of CA signed certificates.
Provide Feedback