Using IP Address and Self-signed Certificates
If you want to use IP addresses you will need to generate self-signed certificates for each of the hosts. Self-signed certificates are untrusted and can cause certificate verification errors if not configured correctly. For this reason the previously described method of using hosts files is preferred.
Additionally, you will need to edit the Security Provider configuration file (fta-setup-env) to include IP addresses for the different FTA services.
Private Network with IP Address

The following overrides would be appropriate for this deployment scenario:
fta-setup-env Setting | Override Value |
---|---|
SECURITY_PUBLIC_IP_ADDRESS | 192.168.1.5 |
DATAVIEW_PUBLIC_ IP_ADDRESS | 192.168.1.5 (for future deployment) |
FLOWML_PUBLIC_ IP_ADDRESS | 192.168.1.5 (for future deployment) |
EDGE_UI_PUBLIC_ IP_ADDRESS | 192.168.1.6 |
EDGE_SERVICES_PUBLIC_ IP_ADDRESS | 192.168.1.6 |
Provide Feedback