Run
fta-remove-admin (Optional)
After running all
of the previous setup scripts and configuring the application client
the master admin account is no longer needed for installation. If
user want to remove the master admin account, run the following
script. If user do not remove the account user must ensure to protect
the account credentials.
|
The master admin account can be recreated in
the future using the fta-setup-admin script. There can only be one
master admin.
Provide Feedback