Create and Start the Security Service
NOTE:
Any adjustments to the default server configuration should be done before creating and starting the service.
Open a command shell (cmd.exe) with elevated privileges or using a local Windows administrator account. Change the working directory to FTASecurity/bin/service.
|
Execute the following to install Security as a Windows service
|
Once the service is installed start the Windows service using
|
Provide Feedback