Run
fta-setup-admin
This script creates
an admin user account that is used by the remaining setup scripts.
The FTA_ENV_SECURITY_PRIMARY_ADMIN_USER and FTA_ENV_SECURITY_PRIMARY_ADMIN_PASSWORD
environment variables must be set before running this script. This
master admin account also allows the user to configure the application
client (example: Redirect URIs).
Execute the following command:
|
After adding the user it will restart the Security
Provider service.
NOTE:
It is recommended that to
use a strong password for the master admin account. Alternatively,
after installing and configuring the Security Provider service the
admin user account can be removed for added security. Running the
script fta-remove-admin will delete the admin account used for the
scripts.
Provide Feedback