Run
fta-setup-dataview
This script creates
the Security Provider client for DataView in the Security realm.
Additionally it creates group and roles used by the DataView application.
Execute the following command:
|
The script also generates two files,
security-realm-public-key.json
and dataview.keycloak.json,
which are required
in future configuration steps.Provide Feedback