Run
fta-setup-flowml
This script creates
the Security Provider client for DataFlowML in the Security realm.
Additionally it creates group and roles used by the DataFlowML application.
Execute the following command:
|
The script also generates two files,
security-realm-public-key.json
and dataflowml.keycloak.json,
which are
required in future configuration steps.Provide Feedback