Download CA Public Key

Download CA Public Key

NOTE:
Skip to “Import CA Public Key” section, if root public certificate is available with the user.
Perform the following steps to download the CA Public Key from Google Chrome Browser:
  1. Open the web browser and type https://<FQDN-hostname>:9043/auth
    CA Public Key
  2. Click [Not secure] and then click [Certificate is not valid].
    Select Certificate
  3. The certificate dialog displays. Go to the Certificate Path tab and select the root certificate as shown in image.
  4. Click [View Certificate] to view the certificate details.
    Certificate Path
  5. The Certificate dialog with certificate details displays, go to the Details tab and click [Copy to File…].
    Certificate - Details
  6. Accept the defaults and click [Next] until the ‘File to Export’ screen displays.
  7. Click [Browse] to select the path and enter the certificate name (ca) to save the certificate to the file system.
  8. Click [Next].
    Certificate - Download Path
  9. The Completing the Certificate Export Wizard screen displays, click [Finish] to export the certificate.
  10. ‘The Export was successful.’ message displays, click [OK] to close the window.
    Certificate - Download
  11. Close the dialog box and verify that the ca.cer certificate is downloaded in the provided path.
    Certificate - Downloaded
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.