CA Public Key
The test certificate created using the private CA scripts are not trusted by web browsers (see below).
If you want to eliminate the browser errors when using the test certificates, the root certificate for the private CA can be imported into the system’s trusted certificate store. Most browsers allow to do this in the advanced settings.
NOTE:
For self-signed certificates, ensure to get the root public certificate (ca.crt) from the certificate authority (CA) and import the certificate into the browser. The root public certificate (ca.crt) is available in the C:\Users\Administrator\.fta-ca\CA directory.
Provide Feedback