Extract New Build

TIP:
This document will refer to %SECURITY_HOME% as the current Security release installed folder.
  1. Stop the Security Provider Service to close connections to the FTASecurity database.
  2. Backup the Security Provider:
    1. It is important to keep a copy of the standalone folder as it contains all of the configuration information used by the Security Provider app server.
    2. Backup the FTASecurity database.
  3. Follow the steps in “Extract the FactoryTalk Analytics Security Package” to extract new release of FTASecurity in a new folder. The original version (2.1.0.59 or 2.2.0.66 or 3.0.1.82 or 3.0.2.91 or 3.0.2.94 or 3.02.00 or 3.03.00 <version>) is installed in a folder next to the new version (4.00.00.<version>).
    Example
    : If the current FTASecurity was installed under
    C:\<Install_Directory>\SCIOSecurity-3.03.00.<version>
    , then the new release of FTASecurity should be installed under
    C:\<Install_Directory>\FTASecurity-4.00.00.<version>
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.