About the FactoryTalk DataMosaix User Interface
This section will help you get familiar with the FactoryTalk DataMosaix user interface.
On the FactoryTalk Hub dashboard, you can find the FactoryTalk DataMosaix tile under the
Operations
Tab.FactoryTalk DataMosaix Tile

You can click the [
] icon on the FactoryTalk DataMosaix tile and add it to favorites.

Add to Favorites

Next time when you log in to FactoryTalk Hub, the
Favorite Apps
tab displays by default. You can view the FactoryTalk DataMosaix tile on the Favorite Apps
tab.FactoryTalk DataMosaix added to Favorites

When you click on the FactoryTalk DataMosaix tile or login directly to FactoryTalk DataMosaix, the FactoryTalk DataMosaix landing page opens. The
Applications
tab displays by default.FactoryTalk DataMosaix landing page

Provide Feedback