FactoryTalk DataMosaix Member Roles
FactoryTalk DataMosaix has six predefined roles. Each role has a separate set of capabilities and privileges. Based on the task a member wants to perform, they are assigned roles. A project admin can change roles of other members.
The following table provides information about a role and the tasks that you can perform with that role.
If you are | You can |
Project Admin |
|
Data Configurator |
|
Data Scientist |
|
Application User |
|
Application Developer |
|
System Admin | Create Custom Roles |
Provide Feedback