Default Roles
There are seven predefined roles. These are designed to give a starting point for an implementation. The table below shows the list of default Roles and the associated capability groups.
Default Role name | Default Capability Groups |
---|---|
Application Developer | FTDM-Grp-Applications |
Applications | FTDM-Grp-GenApplications, FTDM-Grp-Experimental-Machine |
Application User | FTDM-Grp-ViewApp |
Data Configurator | FTDM-Grp-DataSetsManagement, FTDM-Grp-Function, FTDM-Grp- Pipeline, FTDM-Grp-DataModel |
Data Scientist | FTDM-Grp-ContextDiag, FTDM-Grp-3D, FTDM-Grp-Data, FTDM-Grp-Raw, FTDM-Grp-Chart, FTDM-Grp-Media, FTDM-Grp-Experimental-Human, FTDM-Grp-ContextEntity |
Extractors | FTDM-Grp- Extractor |
Project Admin | FTDM-Grp-Project FTDM-Grp-CognlteApllnputValidations, FTDM- Grp-AccessManagement |
When a user needs to create a custom role?
If the default role does not fulfill your requirements, you can create a custom role to suit your needs. Once the customized roles are created, to which corresponding default/custom groups can be assigned. Refer to Create a Custom Role.
NOTE:
Only the Project admin can create custom roles. Default roles are read-only.
Extractor and Application methods accessible by roles
The following tables provide information on the extractors and applications methods that can be accessed by the users with associated roles.
Methods | Roles |
GET List of Extractors | APPLICATION DEVELOPER |
PROJECT ADMIN | |
DATA CONFIGURATOR | |
DATA SCIENTIST | |
APPLICATION USER | |
Delete Extractor | DATA CONFIGURATOR |
Register Extractor | DATA CONFIGURATOR |
Update Extractor | DATA CONFIGURATOR |
Methods | Roles |
GET List of Applications | APPLICATION DEVELOPER |
PROJECT ADMIN | |
DATA CONFIGURATOR | |
DATA SCIENTIST | |
APPLICATION USER | |
Delete Application | DATA SCIENTIST |
Register Application | DATA SCIENTIST |
Update Application | DATA SCIENTIST |
Default Roles and Capability Matrix
The following table provides information about a role and the tasks can be perform with that role.
Roles and Capabilities

Provide Feedback