- Extractors
- Analyze Data
Enable or Disable Features
This section describes how to activate and deactivate a feature in FactoryTalk DataMosaix using the Features tab.
NOTE:
By default, the
FT Optix
feature flag is enabled for newly created projects and does not affect existing projects. If a user has already turned it on or off, the setting will remain unchanged. Provide Feedback