Activate Features

Activate Features

Perform the following steps to activate features:
  1. On the Management Console, navigate to
    Manage Access
    >
    Features
    .
    The Features page displays the available features with a short description and the date they were last updated in the feature management platform.
  2. Toggle the button to turn the selected feature
    Active
    .
    Activate Feature
    You will be notified that the selected feature has been successfully activated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal