Program parameters

A program parameter is an argument that can pass data into and out of a program. Unlike local tags, program parameters are accessed publicly outside of the program. Use program parameters to share data between programs.
Types of program parameters include:
  • Input
  • Output
  • InOut
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.