Add Production Meter

Add Production Meter

Perform the following steps to add the Production Meter to the hierarchy list:
NOTE:
The following point is required to view data on
Production meter dashboard
:
  • Correct tag mapping should be done for production count measurement.
  1. Select the
    Site
    or
    Area
    or
    Work center
    , or
    Work units
    and the [] icon appears.
  2. Click the [] icon and select [Add].
  3. In the
    Add Component
    dialog, select [Production] under
    Meter
    from the left pane and set these parameters:
    • Name
      : Provide the production meter name.
    • Description
      : Provide the description of the production meter.
  4. Click [Add].
    Add Production Meter dialog
The "
Production meter added under Site or Area or Work center or Work units successfully
" message displays.
Related Information
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.