Edit Enterprise Default Unit
Perform the following steps to configure the Default unit at the Enterprise level:
- Select theDefault unittab.
- Click the [
] icon on the required default unit and edit the required fields.
- Click [Save].Enterprise Default unit dialogThe "Unit configuration changes updated successfully" message displays.
Provide Feedback