Add Enterprise

Add Enterprise

Enterprise is the highest in the hierarchy list and each tenant has a single Enterprise.
NOTE:
The following points are required to view data on
Enterprise level dashboard
:
  • For Cost charts, the respective rate schedule should be configured at the Site level.
  • For Emission, the respective emission factor should be configured at the Site level.
  • For Production, energy intensity charts should have correct tag mapping for production count measurement.
  • For more than one resource meter harmonized unit defined at the Enterprise level will be used for displaying data for consumption, intensity & emission.
Perform the following steps to create an Enterprise:
  1. Click the [] icon and select [Configuration].
  2. Click [Add Node].
  3. In the
    Add Node
    dialog, set these parameters:
    • Name
      : Provide the Enterprise name.
    • Currency
      : Select the currency from the drop-down list.
    • Description
      : Provide the description of the Enterprise.
    NOTE: You can configure currency at the Enterprise level.
  4. Click [Add].
The "
Enterprise added to hierarchy successfully
" message displays.
Related Information
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.