Site level: Configure Default Unit
You can edit, add, and delete the Default unit for various resources.
Perform the following steps to edit the resource type details:
- SelectConfiguration>Default unitunder any site.You can view all the available resource types in the default unit tab.
- Click the [
] icon on the required resource type.
- In theEdit unit configurationdialog, edit the fields and click [Save].Edit unit configuration dialogThe "Resource type updated successfully” message displays.
Perform the following steps to add a new resource type:
- SelectConfiguration>Default unit.
- Click [Add] from the bottom-right corner.
- In theAdd unit configurationdialog, set these parameters:
- Resource type:Select the resource from the drop-down list.
- Consumption unit: Select the unit from the drop-down list.
- Consumption decimal place: Select the decimal place from the drop-down list.
- Demand unit: Select the unit from the drop-down list.
- Demand decimal place: Select the decimal place from the drop-down list.
- Click [Add].Add unit configuration dialogThe "Resource type added successfully” message displays.
Perform the following steps to delete the resource type:
- SelectConfiguration>Default unit.
- Click the [
] icon in the required resource type.
- In theDelete unit Configurationdialog, click [Delete].Delete unit configuration dialogThe “Resource type deleted successfully” message displays.
Provide Feedback