Add Site

Add Site

After adding the Region, you need to add the Site.
NOTE:
The following points are required to view data on
Site level dashboard
:
  • Data from different meters which are directly connected to a Site node will be considered for the data aggregation.
  • For consumption and demand charts, the respective resource meter has to be configured with the proper tag mapping.
  • For Cost charts, the respective rate schedule should be configured at the Site level.
  • For Emission, the respective emission factor should be configured at the Site level.
  • For Production and energy intensity charts should have correct tag mapping for production count measurement.
  • Harmonized units are defined at the Enterprise level and will be used to display harmonized consumption, intensity, or emissions data.
Perform the following steps to add a Site under Region:
  1. Select the
    Region
    and the [] icon appears.
  2. Click the [] icon and select [Add].
  3. In the
    Add component
    dialog, select [Site] under
    Node
    from the left pane and set these parameters:
    • Name
      : Provide the Site name.
    • Geolocation
      : Provide the latitude and longitude details of the Site.
      NOTE: After providing the values, use the up-arrow and down-arrow to increase and decrease the values.
    • Timezone
      : Select the time zone from the drop-down list.
    • Currency
      : Select the currency from the drop-down list.
    • Description
      : Provide the description of the Site.
    NOTE: In the Site component, you can configure base details (geolocation, currency, time zone) and configure the default unit, emission factor, rate schedule, and notification.
  4. Click [Add].
The "
Site added under Region successfully
" message displays.
Related Information
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.