Process Value Meter Tag Mapping

Process Value Meter Tag Mapping

After adding the Process value meter to the hierarchy list, perform the following steps for tag mapping:
  1. Select the Process value meter from the hierarchy list and select the
    Tag map
    tab.
  2. Click [Add Tag].
  3. In the
    Tag Map
    dialog, select the necessary data set from the
    Data set
    drop-down list.
    NOTE: The data set is a container for data objects with metadata about the data it contains.
  4. (Optional) Filter the tag name by providing the keyword.
  5. Select the relevant tag name check box from the table and click [Map Tags].
    Tag map dialog
  6. You can select mapped and unmapped tags for tag mapping. If you select mapped tags, an alert message will appear, providing instructions to confirm the remapping. Click on the [] icon to remove tags that are not required to remap.
    NOTE: Data is not modified or deleted during remapping.
  7. To continue with remap, click [Confirm].
    Multiple tag remapping
    Single tag remapping
  8. In the
    Tag map
    dialog, click
    Map Tags
    .
    The "
    Selected tags are mapped to the Process value meter successfully
    " message displays.
    NOTE:
    Once the tag is mapped, make sure to update the mandatory fields (
    Measurement
    and
    Unit
    ) by following the steps 9-11. Failing to do so will cause errors in the dashboard charts.
  9. Click the [] icon beside the tag name and the
    Edit Tag
    dialog is displayed.
    Edit Tag Dialog
  10. Provide the
    Measurement
    and
    Unit
    details and click [Save].
  11. The "
    Tag changes updated successfully
    " message displays.
  12. To remove tags, select the required tag check box from the
    Tag Map
    table.
  13. Click [Remove].
  14. In the
    Remove Tags
    dialog, click [Delete].
    Remove Tags dialog
    The "
    Tag removed successfully
    " message displays.
Related Information
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.