- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Develop a persistent setting specific to a user
Create a check box that shows or hides a clock label, which state is persistent based on the currently logged in user.
Application example

NOTE:
Download a sample project:
UserSpecificPersistentSetting.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select 
Run
Provide Feedback