Manage dynamic links

Manage dynamic links

Use C# APIs to set or remove dynamic links on the variables.
The APIs are supplied by the
IUAVariable
C# class.
TIP: By default, dynamic links defined in a NetLogic are read-only, whereas dynamic links created with the
FactoryTalk Optix Studio
UI are read and write.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.