IUAVariable.ResetDynamicLink()

IUAVariable.ResetDynamicLink()

Remove a dynamic link set on a variable.
void ResetDynamicLink();

Example

The following example shows an API that removes the dynamic link set on the
Text
property (which node is represented by
TextVariable
) of the project object corresponding to
myLabel
:
myLabel.TextVariable.ResetDynamicLink();
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.